SKF Logo White

Meet modern farming challenges with application specific bearings that go the distance

Built for purpose, built to last.

SKF Insert Bearings and Ball Bearing units for agricultural applications

Today's competitive agriculture industry demands greater and more efficient production. However crop residue, moisture, grain, dirt, dust, and all manner of debris can jeopardize farm machinery if it is not properly equipped for the challenge.

Current insert bearings on the market are used across several industries. The problem with these standardized solutions is a lack of performance in tough and demanding operating environments that require specific features for maximum machine life. Fortunately, SKF’s range of insert bearings and ball bearing units have specific features designed for agriculture-specific equipment.

Your bearing unit choice – no matter the size or scale of your farming operation.

Out in the field, standard solutions become substandard. Unless they are equipped with tailored features as displayed, end-users and equipment manufacturers are unlikely to reach maximimum efficency with their machines. This can lead to several costly problems, such as unplanned downtime and lost productivity in the field, as well as expensive repair bills.

By working closely with key agricultural stakeholders from global companies and combining this with SKF in-house knowledge, we are able to provide a solution which supports high integrity, low-maintenance operation.

Economic considerations and unparalleled design characteristics such as the robust sealing technology, are just some of the reasons why SKF insert bearings for agriculture are the ultimate solution for your agricultural application.

Now available in both metric and inch sizes, the SKF insert bearing range offers greater flexibility for your applications.

Increased equipment life

Reduced ownership costs

Reduced downtime

 

Solutions designed specifically for agriculture environments

 

Proven performance, backed by rigorous testing

SKF insert bearings for the agricultural industry have undergone rigorous testing in both the laboratory and the field to validate their integrity in a variety of agricultural machines and applications.

Read the brochure to see how these validation tests prove long‑lasting performance in the field.

SKF Agricultural Insert Bearings: Insights & Innovation

Explore expert insights that show how SKF insert bearings are engineered to perform in agriculture.

Designed to Outlast the Field

SKF’s new bearings range boasts five times the corrosion resistance of other models

Read more

Upgrade to longer‑lasting performance in the field

Please complete the form and a member of the
SKF team will be in touch with you.