× Cookies Information - SKF uses cookies on our web site to align the information shown as closely as possible to the visitors' preferences and to tailor our web site user experience in general. By continuing to visit this site you agree to our use of cookies as described in our cookies policy - www.skf.com/au/footer/cookies

Introducing our agricultural solutions

Working with agricultural technology leaders around the world, SKF,
together with its brand PEER, equip tractors, combine harvesters,
and attachements with products and solutions.

 

What if you could get spare parts when you need them, minimize downtime,
and master the challenges of modern farming?
  

 

With optimally designed components, you can.
Spend more time farming and less time repairing and maintaining, with agricultural equipment that you can rely on - all season long.

How SKF supports companies in the world’s most demanding industry

We provide a variety of solutions and services that help farmers achieve more with less.

Design and upgrade easily: Learn how you can benefit from PEER custom-made solutions.

Innovation and reliability: See how SKF helps farmers reduce maintenance costs and increase uptime

Choose from a large variety of products and solutions designed and selected for the your needs when running agricultural equipment.

BEARINGS
AGRI HUB

Read more

SKF, together with its brand PEER, provides solutions and products for equipment in all stages of the crop cycle, from tillage to crop storage. With a full standard assortment from SKF, complementary and customer-specific solutions from PEER - as well as an increased Agri Hub range - you can achieve high reliability while lowering the total cost of ownership. Choose from an extensive number of SKF spare parts - including PEER designations - available from stock. Gain access to a best-in-class bearing logistic network with global and quick availability.

SKF Agri Hub S20 for seeding

SEALS

Read more

Out in the field, seal failures can lead to several costly problems, such as unplanned downtime, lost productivity, and contaminated soil and crops. Robust sealing solutions from SKF can help withstand the severe contamination common to agricultural applications.

SKF has a wide range of industrial radial shaft seal designs (CR seals) for any focus, rating, and speed requirements. Proven, tried, and tested, there is an SKF seal for almost every agricultural task in every part of the tractor. The products are available from stock and many agricultural equipment distributors are already providing them.

The application-specific products offer a high-performance solution, designed to reduce the need for relubrication, saving precious hours needed for field work. The seal design significantly improves contamination exclusion when compared with conventional triple-lip seal designs.

SKF has recently launched a new generation cassette seals for wheel-end applications of agriculture vehicles. MUD11 is used in the wheel end of tractors, skid steers, wheel loaders which uses oil in their application. The application challenges of long and intense working periods, exposure to harsh contaminated environment provides a perfect opportunity for MUD11 sealing solution, which will help to exclude contamination ingress and loss of lubricant of the wheeFl end.

1. Half-metal/half-rubber outside diameter
Improves static sealing, heat dissipation and retention in housing.

2. Bumper
The bumper positions the sleeve relative to the seal to balance the right interference for the axial lips. It also acts as a line of defence against contaminants.

3. SKF developed nitrile rubber
Represented by all of the light-green areas in the illustration, this standard SKF Mudblock sealing lip material is a unique nitrile rubber compound. Specially formulated by SKF to reduce wear and ageing, this advanced material is compatible with most synthetic oils.

4. Curl
Curled feature closes the unitized design, promotes easier installation and dismounting and also prevents seal disassembly during transport and handling.

5. Main lip
The spring-loaded main sealing lip keeps the sealing lips lubricated and promote sealing ability regardless of rotation direction. This results in less friction and wear for extended service life.

6. Integrated counterface
Wear sleeve and seal form a single, unitized seal unit that eliminates shaft machining requirements.

7. Multiple sealing lips
Pre-greased auxiliary radial and axial lips support the main lip for maximum protection against liquid or solid contaminant ingress.

8. Full rubber inside diameter
Contributes to effective static sealing and helps to reduce the assembly force required for installation.

AGRI CHAIN

Read more

Our brand-new range of agricultural chains are specifically designed to combat the harsh conditions found in farming operations. SKF can add value by providing high quality products at an affordable price. And, on top of that, you gain access to inventory from local warehouses – wherever in the world you are.

Our 98-page catalogue can help you to identify which one is right for you. All chains are fully interchangeable with standard OEM-specification chains and our expert engineers will work alongside OEMs and aftermarket customers to ensure the most suitable chain is properly installed.

LUBRICATION

Read more

Proper manual lubrication normally takes about 30 minutes per machine and maintenance cycle. Failure to properly lubricate each lubrication point on every machine can have a negative impact on schedules, maintenance costs, and equipment performance.

SKF's automatic lubrication solutions for agriculture are designed to drive farm machinery reliability and can keep your machines running throughout the season, without unplanned stops.

SKF offers a complete selection of high-performance lubrication systems for the agricultural market, which are tailored to the customer’s specific requirements.

SKF Lubrication

CONDITION MONITORING

Read more

What if you could extend service life, reduce costly unscheduled downtime and thereby maximize availability even during peak seasons? SKF offers a variety of technology solutions which monitor and diagnose the condition of your farm machines. This can range from the potential fault detection in rotating parts, to automated lubrication practices. practices.

SKF IMx-8 and SKF IMx-16, for example, are compact devices which support proactive maintenance practices and provide a complete system for early fault detection.

SKF QuickCollect is an easy-to-use, bluetooth-enabled sensor which – when used with SKF ProCollect – allows you to check the condition of your components such as bearings, gears, fans, and pumps. Overall data can be viewed in real time or moved to the cloud for future analysis.

Condition Monitoring

SKF and its brand PEER offer solutions for all agriculture machinery – from standard products to special solutions. With a best-in-class-bearing logistic network with global availability, you can get reliable spare parts, when you need them. Get in contact with your local SKF representative today.

Learn more on SKF Agriculture on skf.com